This toolbar provides additional blocks to insert math operations during the Sequence. To add one of these blocks to the Sequence, drag it from the Math Blocks toolbar to the Sequence Workspace.
Settings Menu: The following parameters are available in the Settings menu for most of the math blocks.
| Title | Change the title that appears as the column heading in the Results table. | |
| Color | Change the color of this block. The color of the corresponding information in the chart and table also change. | |
| Save Data | Save data generated by this block and display the data in the Results table. |
Insert a basic math operation with measurement units.
| Block | Description |
| + | Adds the two operands. |
| – | Subtracts the second operand from the first. |
| X | Multiplies the two operands. |
|
|
Divides the first operand by the second. |
Insert a math block with measurement units.
| Block | Description |
| –X | Multiplies the operand by -1 to change the sign. |
|
|
Returns the operand's square root. |
|
|
Returns the square of the operand. |
| abs | Returns the operand's absolute value. |
Insert an exponential or logarithmic block with measurement units.
| Block | Description |
|
|
Raises 10 to the power of the operand. |
|
|
Raises 2 to the power of the operand. |
|
|
Raises e (2.718) to the power of the operand. |
|
|
Raises the first operand to the power of the second. |
|
|
Returns the base 10 logarithm of the operand. |
|
|
Returns the base 2 logarithm of the operand. |
| ln | Returns the natural logarithm of the operand. |
Insert a logic or relational block with measurement units.
| Block | Description |
| and | Returns TRUE if both operands are true |
| or | Returns TRUE if either operand is true. |
| not | Returns the logical opposite of the operand. |
| = | Returns TRUE if both operands are equal. |
| ≠ | Returns TRUE if both operands are not equal. |
| < | Returns TRUE if left operand is less than right operand. |
| > | Returns TRUE if left operand is greater than right operand. |
| ≥ | Returns TRUE if left operand is greater than or equal to right operand. |
| ≤ | Returns TRUE if left operand is less than or equal to right operand. |
Insert a constant block.
| Block | Description |
| ∏ | Returns constant equal to 3.14159... |
| 2∏ | Returns constant equal to 6.28318... |
|
|
Returns constant equal to 1.41421... |
|
|
Returns constant equal to 1.73205... |
| e | Returns constant equal to 2.71828... |
| +Overload | Returns positive overload value. |
| –Overload | Returns negative overload value. |
| True | Returns TRUE. |
| False | Returns FALSE. |
Insert a trigonometric block with measurement units.
| Block | Description |
| sin | Returns the sine of the operand. |
| cos | Returns the cosine of the operand. |
| tan | Returns the tangent of the operand. |
| asin | Returns the arc (inverse) sine of the operand. |
| acos | Returns the arc (inverse) cosine of the operand. |
| atan | Returns the arc (inverse) tangent of the operand. |
| sinh | Returns the hyperbolic sine of the operand. |
| cosh | Returns the hyperbolic cosine of the operand. |
| tanh | Returns the hyperbolic tangent of the operand. |
Insert a time of day block. Returns the time in seconds since January 1, 2016 at midnight.
Insert a block to convert between radians/degrees or Watts/dBm.
| Block | Description |
| rad |
Converts value from degrees to radians. |
| ° |
Converts value from radians to degrees. |
| W |
Converts value from dBm to Power in Watts. |
| dBm |
Converts value from Power in Watts to dBm. |
Insert a statistics block with measurement units.
| Block | Description |
| max | Returns the maximum of two specified values or variables. |
| min | Returns the minimum of two specified values or variables. |
| avg | Returns a running average of the specified variable within a sequence loop block. The value is reset to zero whenever a subsequent AVG block is added to the sequence. |
| sum | Returns the running summation of the specified variable. The value is reset to zero whenever a subsequent SUM block is added to the sequence. |